For Immediate Release
Contact:
mktgcomm@tams.com
TOSHIBA ANNOUNCES THE VANTAGE CGV FOR CARDIAC MRI STUDIES
Ultra-Short Bore MRI System Offers New Gradient Configuration and Applications Dedicated
to Advanced Cardiac Examinations
ACC Booth #3551 Hall D
TUSTIN, Calif., March 8, 2005 – To meet the demands of the U.S.
cardiology market, Toshiba America Medical Systems, Inc. (TAMS) is introducing a
new optimized cardiac configuration for the Excelart VantageTM,
the company’s 1.5-tesla (1.5T) high-field magnetic resonance imaging (MRI) system
equipped with one of the shortest magnets in the industry. Based on the Vantage
XGV platform, the new Vantage CGV configuration features gradient strength of 30
mT/m (milliTesla per meter) and a slew rate of 130 mT/m/ms (milliTesla per meter
per millisecond) to meet clinical requirements for advanced cardiac MRI examinations.
“With the introduction of the new cardiac configuration for the Vantage line-up,
Toshiba is further expanding our presence in the 1.5T high-field MRI category with
a dedicated system designed to meet the clinical demands of the expanding cardiology
market,” said Bob Giegerich, MRI Business Unit, Toshiba America Medical Systems,
Inc. “In addition to a list of exclusive patient-focused features of the Vantage,
the new Vantage CGV adds advances, such as a specialized cardiac coil, and application
packages for high-resolution cardiac imaging and quantification analysis.”
The Vantage CGV features the latest technology and applications optimized to perform
advanced cardiac MRI procedures, including eight-channel radio frequency (RF) electronic
components, Toshiba’s cardiac/torso SPEEDER coil, and software packages designed
for high-quality cardiac MRI studies, including Respiratory, Peripheral Pulse and
Cardiac Gating. The new cardiac configuration also enables freeze-frame imaging,
Differential Rate K-space Sampling (DRKS), a SPEEDER-compatible, high-resolution,
time-resolved MR angiography (MRA) technique with temporal resolution as low as
0.6 seconds when combined with the cardiac SPEEDER coil. Additionally, the
new system incorporates a PC-based workstation to operate the MEDIS MRI-MASS® (MR
AnalyticMulti-View allows visualizational Software Systems), an industry leading
cardiac quantification analysis application, and an in-room Gating Monitor mounted
to the gantry to allow evaluation of the cardiac cycle while positioning the
patient.
Unmatched MRI Performance and Patient-Focused Features
The Vantage features one of the industry’s shortest magnets at 140 cm with linear
30 mT/m gradient strength and a slew rate 130 mT/m/ms for the Vantage CGV.
Despite the short length of the magnet, the system delivers the highest homogeneity
of any magnet in the industry within a full 50 cm diameter spherical volume (DSV).
With Toshiba’s patented PianissimoTM technology,
which effectively reduces acoustic noise by as much as 90 percent, the Vantage significantly
reduces the most significant cause for patient discomfort and enables clinicians
to better utilize the system’s high-field MRI capabilities and SPEEDER parallel
processing for increased imaging acquisition speed and reduced exam times.
For more information about the Vantage MRI, TAMS and its wide range of medical imaging
products, please visit our Web site at www.medical.toshiba.com.
About Toshiba
With headquarters in Tustin, Calif., Toshiba America Medical Systems markets, sells,
distributes and services diagnostic imaging systems, and coordinates clinical diagnostic
imaging research for all modalities in the United States. Toshiba Medical
Systems Corporation, an independent group company of Toshiba Corporation, is a global
leading provider of diagnostic medical imaging systems and comprehensive medical
solutions, such as CT, X-ray, Ultrasound, Nuclear Medicine, MRI and information
systems. Toshiba Corporation is a leader in information and communications
systems, electronic components, consumer products, and power systems. Toshiba
has approximately 161,000 employees worldwide and annual sales of $53 billion.
Excelart VantageTM and PianissimoTM are
trademarks of Toshiba Medical Systems Corporation.
MEDIS MRI-MASS is a registered trademark of LUMC.