For Immediate Release
Contact:
mktgcomm@tams.com
TOSHIBA AMERICA MEDICAL SYSTEMS LAUNCHES COILS FOR VANTAGE MRI SYSTEMS
Long Bone Coil and 32 Channel Head/Spine Coil Previewed as Works-in-Progress
RSNA Booth #
7114 (North Building, Hall B)
CHICAGO, Nov. 29, 2005 – Supporting its ongoing commitment to the
development of technologies that meet clinician needs, Toshiba America Medical Systems,
Inc. (TAMS) today announced the launch of two new coils. The first coil is
designed for long bones, such as the humerus and femur, is especially beneficial
when imaging the spine on hard-to-move patients or those suffering from spine disorders
like kyphosis, a permanent curvature of the spine. A new 32-channel head/spine
coil will be available for demonstration and is designed specifically for brain,
cervical, thoracic and lumbar imaging in trauma or immobile patients—delivering
high-resolution images without the need to change coils or move the patient.
Available on
any Vantage MRI system, the new coils will be exhibited as works-in-progress at
the Radiological Society of North America’s (RSNA) annual meeting held Nov. 27-Dec.
2 at McCormick Place in Chicago (Booth #7114, North Building, Hall B).
“Improving patient
positioning has a direct effect on image quality, and we are dedicated to providing
the tools clinicians need to generate the best possible outcomes,” said Bob Giegerich,
director, MR Business Unit, TAMS. “Each of these new coils serve a distinct
purpose in the clinical setting and provide a direct benefit to patients.”
Vantage
MRI—Unmatched Performance and Patient-Focused Features
The Vantage features an ultra-short magnet at 140 cm with linear 30 mT/m (milliTesla
per meter) gradient strength with a slew rate of 50 T/m/s (Tesla per meter per second)
(AGV), 86 T/m/s (MGV), 130 T/m/s (XGV), or 33 mT/M, 200 T/m/s (ZGV works-in-progress).
Despite the short length of the magnet, the system delivers the highest homogeneity
of any magnet in the industry over the full 50 cm diameter spherical volume (DSV).
The Vantage also
offers some of the most advanced MRI applications available on the market today,
including optional packages for cardiac imaging, advanced Echo Planar Imaging (EPI),
Perfusion and Diffusion Imaging, Peripheral MRA, and SuperFASE (Fast Advanced Spin
Echo) imaging. In addition, Toshiba has pioneered research into contrast-free
MRA with its Fresh Blood Imaging (FBI) protocol and Body Diffusion.
With Toshiba's
patented PianissimoTM technology, which reduces acoustic
noise by as much as 90 percent, the Vantage dramatically reduces the most significant
cause of patient discomfort and enables clinicians to better utilize all of the
system's high-field MRI capabilities including SPEEDER parallel imaging for increased
acquisition speed that reduces examination times. For more information about
the Vantage, TAMS and its wide range of medical imaging products, visit
www.medical.toshiba.com.
About
Toshiba
With headquarters in Tustin, Calif., Toshiba America Medical Systems markets, sells,
distributes and services diagnostic imaging systems, and coordinates clinical diagnostic
imaging research for all modalities in the United States. Toshiba Medical
Systems Corporation, an independent group company of Toshiba Corporation, is a global
leading provider of diagnostic medical imaging systems and comprehensive medical
solutions, such as CT, X-ray, Ultrasound,
Nuclear Medicine, MRI and information systems. Toshiba Corporation is a leader
in information and communications systems, electronic components, consumer products,
and power systems. Toshiba has approximately 161,000 employees worldwide and
annual sales of $53 billion.
Excelart VantageTM and PianissimoTM are
trademarks of Toshiba Medical Systems Corporation.